Swagelok Source Inlet
The source inlet establishes a connection between the high-pressure gas source and the rest of the gas distribution system. To ensure the gas can be safely fed into the primary gas pressure control or automatic changeover, it is imperative that the system is built correctly with the necessary bottle connections, hoses, tubing, filters and vent, purge and relief functions.